Accidents (per mio. working hours)*

​​​​

Injuries are measured in amount of injuries, which has caused lost working hours for at least one day after the injury. It is indexed in relation to the amount of 1 mio. working hours.

Number of injuries measured in relation to working hours is reduced by 28% compared with 2008. The actual number of injuries was 232 in 2011.

Please note that comparison figures for year 2008 and 2010 have been changed since reported for the first time. Changes in the indicator, number of injuries, is caused by enhanced data measurement and a more complete scope of working hours. Changes have a moderate impact on trends.

*Deloitte has performed a review of Grundfos Environment, Health and Safety data 2011.

See auditor's statement.

 





    Facebook Twitter LinkedIn Technorati