Pretraživanje enciklopedije

Ponovna pretraga
Prikazujemo 11 do 14 od 14 rezultata
Mixing loop, single shunt with 3-way valve in flow pipe
A single shunt mixing loop is used when variable flow or variable temperature or both are desired on the secondary side.
Mixing loop, single shunt with 3-way valve in return pipe
A single shunt mixing loop with 3-way valve in return is used when variable flow is desired on the secondary side and variable temperature is undesirable.
Modbus
Modbus is an open network technology used in building management systems and across a wide range of industries. It is a de facto standard for data communication, which makes it ideal for use on all automation levels.
Motors
The overall energy efficiency of pumps is derived from the usage of motors. The EuP Directive states that from June 16th 2011, motors sold in the European Union must meet the IE2 efficiency level.